Search
Languages

Bourns Further Expands its Discrete TVS Diode Product Line

RIVERSIDE, Calif., October 21, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the further expansion of its industry-leading line of discrete transient voltage suppressor (TVS) diode products with two new series of ESD/EFT surge protection products. Bourns designed its Model SMA6J and Model SMA6J-Q TVS diodes to protect power buses and I/O interfaces in data lines and DC power supplies. In addition, Bourns® Model SMA6J-Q is AEC-Q101 compliant and well-suited for a broad range of communications, industrial and consumer electronics applications that are used in certain harsh environments and require high reliability.

Both model series come in a compact, industry standard DO214-AC (SMA) package, and feature increased peak pulse power (PPP) dissipation of 600 watts compared to the 400-watt industry standard. TVS diodes are typically rated for peak pulse power allowing designers to determine the best type required for a particular application and environment. These unidirectional/bidirectional devices offer reverse standoff voltage of 5 – 43 V. The features of Bourns' new TVS diodes help enable power supply designers to meet their both their high-power density and small form factor requirements.

Bourns® Models SMA6J and SMA6J-Q are available now and are RoHS* compliant. For additional product information, please see: www.bourns.com/products/diodes/diodes-aec-q101-compliant

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf