MENU
Search
Languages

Bourns Releases Additional LAN 10/100/1000 Base-T Transformer Designed for Ethernet Applications with PoE Function

Riverside, Calif., October 7, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today released an additional LAN 10/100/1000 Base-T Transformer model designed specifically for Ethernet-based applications with Power-over-Ethernet (PoE) functionality. This latest model delivers an extended operating temperature (-40 to +85 °C) making it ideal for harsh environment applications. Designated Bourns® Model SM51589PEL, the company's new LAN transformer can be used as an alternate component to Bourns' existing Model SM51589EL. In addition, Bourns' Model SM51589EL is compliant with IEEE802.3 standards and features 5K VAC dielectric withstanding voltage.

"Bourns is committed to serving our customers with the broadest portfolio of leading LAN 10/100 Base-TX transformer solutions. This latest model is well-suited to meet the rugged, extended temperature operation requirements of LAN, Ethernet and PoE applications," said Guido Zehnder, product manager at Bourns, Inc. "Offering a LAN transformer featuring 5 kVrms voltage, Bourns helps ensure OEMs meet the safety isolation requirements of high-voltage systems."

Pricing and Availability RoHS compliant*, the Bourns® Model SM51589PEL is available now. As a pricing reference, it is priced at $ 1.40 each in 1000 piece quantities. For more information, please see Bourns' Transformer – LAN product page.

关于美国柏恩(Bourns)

Bourns — 是电子零组件业界的龙头制造供货商,公司总部位于美国加州的河边市,其产品包含:位置与速度传感器、电路保护解决方案、磁性组件、微电子模块、面板控制器及电阻产品,服务产业涵盖汽车、工业、消费、通信、非关键性的生命支持医疗(低/中风险)、音频以及其他各种市场。如需了解更多的公司与产品讯息,欢迎上公司网站查询:www.bourns.com