Search
Languages

CenTech, Inc. Marks 55 Years Representing Bourns Across Missouri, Kansas, Nebraska, and Southern Illinois

PR Image
Bourns presented Avnet with the 2025 Bourns Americas Channel Recognition — 55-Year Representative Milestone award at EDS 2026, Resorts World Las Vegas, May 20, 2026.
Pictured from left: Al Yost, President & COO, Bourns, Inc.; Gordon Bourns, CEO, Bourns, Inc.; Dennis Stepanek, President, CenTech; Rich Sartori, VP, CenTech; Jim Harrington, Sr. VP Worldwide Sales, Bourns, Inc.; and Jerry Durand, VP of Sales – Americas, Bourns, Inc.

CenTech has represented Bourns to avionics, government, medical, military, and aerospace customers across four states since its founding year.

LAS VEGAS, Nevada, May 26, 2026 - Bourns has recognized CenTech, Inc. for 55 years as a Bourns manufacturer’s representative. The milestone was acknowledged during EDS 2026 at Resorts World Las Vegas as part of Bourns’ annual Americas channel recognition program, which has honored outstanding distributor and representative relationships since 2014.

CenTech was founded in 1969 to provide professional technical sales representation for electronic component manufacturers and took on Bourns as a principal in its first year of operation. The firm covers Missouri, Kansas, Nebraska, and Southern Illinois from offices in Lee’s Summit and St. Louis, calling on avionics, government, medical, industrial, military, and aerospace accounts where component selection is specification-driven, and supplier relationships are long-term. The representative relationship, active since 1970, continues across the same four-state territory today.

“Fifty-five years is rare in this industry. CenTech has been in front of the right customers in Missouri, Kansas, Nebraska, and Southern Illinois for more than five decades. The relationship works because they know the Bourns portfolio and they know their customers — and that combination is not easy to replace.”
— Jerry Durand, Vice President of Sales – Americas, Bourns

Milestone Highlights
  • Tenure — 55 consecutive years representing Bourns; the relationship began in 1970, CenTech’s first full year of operation.
  • Firm founded — 1969, Lee’s Summit, Missouri.
  • Territory — Missouri, Kansas, Nebraska, and Southern Illinois, served from offices in Lee’s Summit and St. Louis.
  • Bourns product lines — passive and electromechanical components across power, protection, and sensing, serving CenTech’s avionics, defense, medical, and industrial customer base.

“Fifty-five years means we’ve seen this territory through multiple cycles — the customer base has changed, the products have evolved, and the relationship has held. What makes it work is straightforward: we know the Bourns portfolio, we know our customers, and we show up. That’s been true since 1970, and it’s still true today.”
— Dennis Stepanek, President, CenTech, Inc.

About CenTech, Inc.

CenTech, Inc. is an independent manufacturers’ representative firm founded in 1969 and headquartered in Lee’s Summit, Missouri, with an additional office in St. Louis. CenTech provides professional technical sales representation for electronic component manufacturers across Missouri, Kansas, Nebraska, and Southern Illinois. For more information, visit centech-inc.com.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com