Search
Languages

Bourns Announces High Power Metal Strip Current Sense Resistors in Compact SMD 2010 Package

Automotive grade, AEC-Q200 compliant current sense resistors are designed for applications requiring a small size, accurate resistance value and resistance tolerance

RIVERSIDE, Calif., July 8, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced an extension of its CRF Series automotive grade, AEC-Q200 compliant current sense resistors to be available in a compact surface mount (SMD) 2010 package. Bourns designed the CRF2010 model to meet the small size, accurate resistance value and resistance tolerance requirements in Battery Management Systems (BMS), Switch-Mode Power Supplies (SMPS), motor control, Electric Vehicle (EV) board net current control, inverter phase current sensing and for robotic current control applications.

In addition, Bourns is making its Model CRF2512 Current Sense Resistors in the 2512 SMD package size available in a high power 3 W version. The Model CRF2512 is AEC-Q200 compliant and features resistance values as low as 0.0003 ohms with an inductance of less than 5 nanohenries (nH). These features make this new 3 W version ideal for power supplies, stepper motor drives and input amplifiers.

The new Model CRF2010 supports resistance tolerances of 1 % and 5 % with a fixed TCR value of ±50 ppm/° C, and supports resistance ranges from 1 mΩ to 50 mΩ with the same TCR. These current sense resistors also boast an excellent 1.5 W power rating in a compact size. In addition, the series’ metal strip construction enables smaller, thinner package sizes, and offers superior surge energy resistance compared to typical 2010-sized resistors with the added value of providing automotive-grade reliability for demanding applications.

The Bourns® CRF2010 Series and CRF2512 Series High Power Current Sense Resistors are available now through Bourns’ authorized distribution partners, and are RoHS* compliant. For more detailed product information, please see: bourns.com/products/resistors/current-sense-resistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf