Search
Languages

Bourns Releases Two Compact NTC Thermistor Series Offering High-Precision Temperature Sensing and Compensation

The Bourns® BTN02G and BTN04G Series provide essential and highly accurate thermal management for today’s sophisticated and sensitive electronics applications

RIVERSIDE, Calif., June 4, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its BTN02G and BTN04G Series SMD Negative Temperature Coefficient (NTC) Thermistors. Designed as a high-precision and compact temperature sensing and compensation solution, Bourns’ new NTC thermistors provide essential thermal management for today’s more sophisticated and sensitive mobile devices, home appliances, Li-ion battery packs, LCD displays and other electronic equipment.

These new thermistors feature resistance that is inversely proportional to the temperature, enabling accurate temperature measurement. The advanced and high reliability design of the BTN02G and BTN04G series combines semiconducting ceramics and internal electrodes, providing the capability to uniformly and smoothly change resistance values over a wide temperature range. In addition to the standard ±3 percent and ±5 percent high-precision resistance tolerances, Bourns’ latest NTC thermistors are also available in ±1 percent and ±2 percent resistance tolerances. The series’ B-Value tolerance is highly accurate at ±1 percent, making them superior temperature sensing solutions.

Bourns® BTN02G and BTN04G Series SMD NTC Thermistors are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/thermal-sensing-devices/ntc-thermistors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf