Search
Languages

Bourns Offers its SSD Series Digital Current Sensors with Internal 120 Ohm Resistor Option

The resistor option provides impedance matching, signal reflection prevention and enhances signal integrity in applications that employ Bourns® high-accuracy digital DC current sensors

RIVERSIDE, Calif., April 29, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that it is now offering its SSD Digital Current Sensor Series in both the CANbus and RS-485 versions with an internal 120 ohm (Ω) resistor option. With this new option, designers get additional impedance matching and signal reflection prevention benefits that aid in ensuring robust communication. Using the Bourns® SSD Digital Current Sensors with the resistor option assists in maintaining signal integrity, especially over longer distances and at higher speeds, while helping to prevent communication errors. Bourns® SSD Digital Current Sensors offer superior accuracy, stability and electrical isolation over a wide - 40° C to +115° C operating temperature range even in certain harsh industrial and automotive environments. The series feature 1500 VDC reinforced galvanic isolation, a 16-bit +150 °C microcontroller, a 24-bit ADC with buffered analog inputs and ECC flash memory with autocorrect single-bit error capability. These advanced features make them excellent solutions for battery systems, renewable energy, motor drives and EV charging stations.

The new internal 120 Ω termination resistor option is constructed in the PCB of the sensor and is available now in nominal current values of 100A, 250A and 500A. The Bourns® SSD Digital Current Sensor series is RoHS* compliant. For more detailed product information, please see: bourns.com/products/sensors/current-sensors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf