Search
Languages

Bourns Expands Digital Current Sensor Line with 500 Amp Series Meeting High Accuracy Measurement Needs in a Wider Range of Applications

The Riedon™ Model SSD-500A Current Sensor – Digital by Bourns offers a precision 24-bit isolated current sensor with CANbus or RS-485 interface options

RIVERSIDE, Calif., December 2, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the release of the Riedon™ Model SSD-500A Series Current Sensor – Digital by Bourns with 500 Amps nominal current. The extended electrical rating allows designers to use a supply voltage of 24 V (15 mA typical), enabling them to meet high accuracy measurement requirements in a wider range of battery-related applications, including large-scale energy storage banks, renewable energy generation infrastructure, industrial motor drives, building automation systems, and EV charging stations.

The Model SSD-500A Series includes advanced digital DC shunt-based current sensors that deliver superior accuracy, stability, and electrical isolation in certain harsh industrial environments. The series also features an internal 24-bit Analog-to-Digital Converter (ADC) that offers plug-and-play simplicity, enabling designers to quickly add high-accuracy current measurement into new designs or retrofit existing ones. These shunt-based sensors also help eliminate the need for periodic device calibrations while also contributing to more efficient use of power. Furthering their design flexibility, the Model SSD-500A Series is offered in RS-485 and CANbus interface options.

The Riedon™ Model SSD-500A Series Current Sensor – Digital by Bourns is available now, and is RoHS* compliant. For additional information, please see: www.bourns.com/products/sensors/current-sensors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf