Search
Languages

Bourns Announces New Low Profile Line Filter Series that Features a 2.5 mm Profile

Bourns® Model SRF0502 Series line filters provide necessary EMI suppression helping to maximize system uptime in mission-critical applications

RIVERSIDE, Calif., October 28, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new low profile line filter series. Featuring a compact 2.5 mm profile, Bourns® Model SRF0502 Series line filters are designed to meet a variety of customer requirements. This new series provides EMI (Electromagnetic Interference) suppression for mission-critical applications where interference must be minimized.

In addition to its low profile design, Bourns® latest line filter series features a shielded construction that further helps to minimize EMI while delivering low DCR, a high current rating up to 5 A and a frequency range up to 700 MHz. These line filters are ideal common mode power choke solutions for eliminating noise in a range of industrial power supplies and other applications that demand high reliability operation.

The Bourns® Model SRF0502 Series line filters are available now and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/common-mode-chokes.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf