Search
Languages

Bourns Introduces BMS Signal Transformer Optimized for Higher Energy Storage Battery Management System Applications

Bourns® Model SM91801AL is developed for use with Analog Device Model LTC6815 Series, NXP Model MC33771C Series and Texas Instruments Model BQ79616

RIVERSIDE, Calif., February 28, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today introduced a new single channel basic insulation transformer with a planar structure optimized for Battery Management System (BMS) applications. Bourns® Model SM91801AL is the next ‘first to market’ BMS signal planar transformer product Bourns has engineered, and is developed for use with several prominent semiconductor supplier IC series: Analog Device Model LTC6815 Series, NXP Model MC33771C Series and Texas Instruments Model BQ79616 ICs that are primarily used in multi-cell battery monitoring designs.

The latest BMS planar signal transformer from Bourns is AEC-Q200 compliant and automotive grade. It features a basic insulation layer that complies with IEC 60664-1 and IEC 62368-1 standards, and is manufactured using a fully automated process to deliver a high quality and cost-effective solution for next-generation applications. This BMS transformer offers a working voltage of up to 1000 VDC and a Hi-Pot isolation voltage up to 4300 VDC or 2500 VAC with an extended operating temperature range of -40 to +125 °C.

Bourns® Model SM91801AL is available now and is RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/transformers-bms-aecq200.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf