Search
Languages

Bourns Introduces 12mm Dual Concentric Rotary Encoder Series Featuring Two Encoders in a Single Package

Model PEC11D series offers a high reliability solution that addresses space constrained design requirements in a wide range of applications

RIVERSIDE, Calif., January 24, 2022 - Bourns, Inc., a leading manufacturer and supplier of electronic components, , today introduced a new 12mm dual concentric rotary encoder series that features two encoders in a single package. Bourns® Model PEC11D allows designers to specify a single encoder in applications that require the functionality of two encoders. With a high IP40 seal rating, a 15,000-rotation life rating and a –40 to +85 °C operating temperature, Bourns® Model PEC11D Series offers a high-reliability solution for a wide range of applications including professional audio and lighting, communications, test and measurement equipment, low/medium risk medical** diagnostic and laboratory equipment as well as for industrial automation controls.

Built with a metal bushing and metal dual concentric shaft, the new encoder series from Bourns features a two-bit quadrature output that allows for phase and direction information. This series also has a momentary push switch with a 20,000-cycle rated switch life and two switch options – high and standard stroke – in otherwise identical package dimensions. The switch options enable the encoder to adapt to individual customer needs and application environments.

"Bourns led the market more than 70 years ago with a breakthrough potentiometer design that helped enhance instrumentation capabilities. Our new dual concentric rotary encoders with switch are an example of the Company's ongoing commitment to developing innovative quality products with advanced features," said Alain Leon, Sensors Product Line Manager at Bourns. "This is our first dual concentric rotary encoder that has been specifically designed to meet today's board density requirements."

The Bourns® Model PEC11D encoder series is available now and is RoHS compliant*. For more detailed product information, please see: www.bourns.com/products/encoders/contacting-encoders

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf