Search
Languages

Bourns Announces AEC-Q200 Compliant and Sulfur-Resistant Thick Film Chip Resistor Array Model Families

The Model CAYxxA-AS series are the first chip arrays from Bourns that are both AEC-Q200 compliant and sulfur-resistant based on ASTM-B-809-95 and EIA-977 standards

RIVERSIDE, Calif., April 13, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced several new AEC-Q200 compliant thick film chip resistor array model families. Bourns designed the new surface mount model CATxxA-LF, CAYxxA-LF and CAYxxA-AS series to help increase available board space and reduce costs. Offering long-life protection against many sulfurous environments, the Model CAYxxA-AS series are the first chip arrays from Bourns that meet both the AEC-Q200 standard and anti-sulfur protection requirements based on the ASTM-B-809-95 and EIA-977 (test parameter B) standards making them superior circuit conditioning solutions for a wide range of transportation, consumer electronics, industrial automation, power supply and LED lighting and communication base station applications that must operate in extreme conditions.

These latest resistor families from Bourns are constructed using a thick film element printed onto a ceramic substrate, which allows for a wide resistance range and increased design flexibility in terms of size and dimensions. The new AEC-Q200 compliant Model CATxxA-LF concave and CAYxxA-LF and CAYxxA-AS convex chip arrays are available in 1 mm and 1.6 mm widths and contain two or four pieces of isolated thick film resistive elements printed onto a single ceramic substrate.

Bourns® Model CATxxA-LF, CAYxxA-LF and CAYxxA-AS Series are available now and are RoHS* compliant. For additional product information, please see: www.bourns.com/products/resistors/chip-resistor-arrays

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf