Search
Languages

Bourns Upgrades Line of Humidity Sensors Based on MEMS Technology with New Model Series

New humidity sensor series meets advanced sensor needs with fast response time, high accuracy/sensitivity in a small footprint

RIVERSIDE, Calif., March 30, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new model in its line of environmental sensors based on Microelectromechanical Systems (MEMS) technology. The new BPS240 series offers upgraded features compared to Bourns® BPS230 humidity sensors. The enhanced features include a faster response time of less than one second with digital (I2C) output and higher accuracy with a typical RH accuracy of 2 percent. Bourns' latest humidity sensor model family also deliver reliability in a small size (2.0 x 2.0 x 1.25 mm) footprint.

The Model BPS240 series is designed to meet advanced sensor needs for immediate updates on relative humidity levels in a broad range of industrial automation, energy, building & home control and low/medium-risk medical*** applications. The sensor series also helps meet energy-efficient application requirements with its low voltage operation, reduced current consumption and reliable embedded capacitive technology.

"In addition to the upgraded features we engineered into the new BPS240 series, Bourns is known for our proven history of excellent customer technical support, the time-to-market advantages we can deliver from our comprehensive channel presence, and added product confidence from our quality system certification," said Alain Leon, sensors product line manager at Bourns, Inc.

The new Bourns® Model BPS240 humidity sensor series is available now and is RoHS compliant*. For additional product information, please see: www.bourns.com/products/sensors/environmental-sensors

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf