Search
Languages

Bourns New Hybrid Surge Protective Device Offers Multi-Mode Protection in a Compact Design

RIVERSIDE, Calif., January 6, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the Bourns® Model 1202 Series. This Type 1 hardwired hybrid surge protective device (SPD) is designed for AC infrastructure applications. Bourns engineers have combined the company's fast-responding Metal Oxide Varistor (MOV) technology with its low leakage Gas Discharge Tube (GDT) technology to deliver a device that provides consistent, long-life, reliable and enhanced protection performance. The Model 1202 Series employs a full multi-mode protection scheme that can be utilized in line-to-line, line-to-neutral and neutral-to-ground configurations.

The innovative hybrid design uses the GDT to isolate the MOV from the line voltage thus shielding it from transients and temporary overvoltage spikes that can potentially damage the MOV over time. The GDT's ultra-low leakage also helps to reduce damage due to watt loss heating.

The Model 1202 has a nominal current rating of 10 kA and a short circuit current rating of 25 kA. The device's LED indicators provide visual indication when the surge protector encounters any situation that requires its internal safety fusing to activate. In addition, the Series is IP66/NEMA 4x rated and can be used indoors or outdoors. As a Type-1 SPD, the Model 1202 requires no external line fusing or circuit breaker, and can be placed on the line side of the main service disconnect. The extensive features designed into Bourns' latest hybrid SPD make it an optimal solution to protect against lightning threats, up to rated limits, and for AC power-induced problems in applications such as service entrances, branch and OEM panels, electrical infrastructures and in equipment and systems cabinets.

Available now, Bourns® Model 1202 Series is available in a 120 Vrms version as well as a 120/240 Split Phase version. Both models are RoHS compliant* and listed to UL 1449, Issue 4. For additional product information, please see: www.bourns.com/docs/product-datasheets/1202.pdf

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com