Search
Languages

Bourns Expands Line of Environmental Sensors with Ultra-Low 0.15 PSI Pressure Sensor Models

RIVERSIDE, Calif., February 4, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the expansion of its line of environmental sensors adding an ultra-low 0.15 to 1.0 PSI pressure sensor. Bourns® Models BPS110/BPS120 pressure sensors are based on state-of-the-art Micro-Electro-Mechanical Systems (MEMS) technology, which provides extremely accurate condition readings in a miniature package size. Designed to deliver superior performance in applications where precision is essential, Models BPS110/BPS120 offer fully calibrated and compensated output for more efficient processes as well as long-term stability for reliable repeatability. These features make Bourns' new pressure sensor an ideal solution for a range of industrial, consumer and medium/low-risk medical* designs including portable oxygen generators, nebulizers, CPAP equipment, diagnostic spirometers and gas chromatography equipment.

"What sets Bourns apart is our strict attention to quality and expert technical support all backed by Bourns' global supply chain," said Alain Leon, Sensors & Controls Product Line Manager at Bourns, Inc. "Another benefit is we are able to leverage Bourns' decades of medical market experience in meeting new application needs for highly accurate, miniaturized and sensitive sensor technologies that help designers advance and expand healthcare device and equipment usage."

Bourns Models BPS110/BPS120 feature extreme sensitivity and stability with a Total Error Band (TEB) of 1.5 % FS over a temperature range of 0 °C to +60 °C (Six-Sigma process), and lifetime drift of 0.5 % FS. The new sensor models help to minimize system calibration needs, and help support system uptime. Its compensated plug and play shorten development time, and offers excellent design flexibility for use in either analog (BPS110) or digital systems (BPS120) where an amplified, calibrated pressure signal can be acquired from the digital interface or analog output.

See Bourns Models BPS110/BPS120 pressure sensors and the company's entire line of BPS environmental sensors at MD&M West, February 5-7, 2019 in booth #948.

Bourns Models BPS110/BPS120 pressure sensors are available now. Bourns also offers port configuration and calibration customization. For more detailed product information, please go to: www.bourns.com/docs/technical-documents/technical-library/sensors/publications/Bourns_BPS110_and_120_Product_Brief.pdf.

* *Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice https://www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf