Search
Languages

Bourns Acquires Assets of Polymer PTC Business of Therm-O-Disc, Inc.

RIVERSIDE, Calif, July 26, 2006 - Bourns, Inc. is pleased to announce the acquisition of the principal assets of the Polymer PTC division of Therm-O-Disc, Inc. (T-O-D), including equipment, intellectual property and backlog. Terms were not disclosed.

T-O-D, headquartered in Mansfield, OH, with additional manufacturing in Shenzhen, China, has earned a solid reputation for the design and manufacture of Polymer PTC devices for the protection of DC-motors, particularly for automotive applications.

Bourns is a leading supplier of Circuit Protection solutions with an outstanding reputation for the design and supply of technology-leading polymer PTCs for a variety of applications. As an established Circuit Protection and Automotive supplier, Bourns offers a breadth of products unmatched in the passive electronics industry. This acquisition further expands Bourns’ existing Multifuse® Polymer PTC product line manufactured in Bourns’ TS16949 certified facility in Xiamen, China.

"We are very excited about this acquisition. T-O-D has enjoyed excellent print positions with many well established DC-motor manufacturers. Bourns will now be able to combine this strength with its previously launched High Temperature PTC material, which is so highly desired in automotive applications, to strengthen Bourns’ position as a leading PTC solutions provider," commented Dr. Erik Meijer, Vice President of Bourns Circuit Protection. Dr. Meijer said that Bourns plans to transfer the acquired production lines to its PTC plant in Xiamen, China.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf