MENU
Search
Languages

Safety Issues with Counterfeit Bourns® Trimmers!

RIVERSIDE, CA, July 1, 2005

Customers Beware!

Bourns, Inc. has witnessed an increase in the availability of counterfeit and cloned Bourns® trimming potentiometers worldwide. Purchasers of counterfeit or cloned trimmers should be aware of the following risks:

  1. Counterfeit and Clone Manufacturers may not abide by RoHS legislation or provide compliant product;
  2. Counterfeit Manufacturers do not abide by national and international laws protecting registered trademarks;
  3. Counterfeit and Clone Manufacturers likely will not be willing to provide material data sheets or disclose third party material declarations; and
  4. Counterfeit and Clone Manufacturers likely will not have reliable information on newly required tin whisker testing results.
Purchasers of counterfeit or cloned trimmers probably are not aware whether the material used in counterfeit or cloned trimmers complies with applicable safety standards. Any use of non-compliant material should be of significant concern to purchasers of counterfeit or cloned trimmers. For example, we have posted below a video of flammability testing of a genuine Bourns® trimmer and a counterfeit trimmer. This video clearly shows that the housing material in the counterfeit trimmer does not comply with UL-94V0 requirements for flammability resistance thus creating a potentially unsafe condition.

Trimmer Flammability Testing

Fake

Genuine Bourns® Product

For our customers' protection, Bourns recommends that all customers purchase Bourns® products only from authorized Bourns distributors to ensure delivery of genuine products. Authorized Bourns Distributor links are located on the Bourns website at Sales Locations.

Please feel free to contact technical support for more information.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com