Search
Languages

Bourns® IsoMOV® Hybrid Protectors Earn IEC 61051-2 Certificate of Conformity and are UL 1449 Listed

With features that extend application service life and enhance reliability, IsoMOV® protectors are the first hybrid surge protection devices to receive both global standards

RIVERSIDE, Calif., May 1, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its innovatively designed IsoMOV® hybrid protectors have earned the IEC 61051-2 Certificate of Compliance and are UL 1449 listed. Bourns® IsoMOV® protectors are the first hybrid surge protection devices to have met the stringent tests and documentation required by these global standards. Now, designers can confidently add the longevity and high reliability benefits IsoMOV® protectors provide to a growing group of key market applications where IEC certification is a prerequisite.

“Earning the IEC Certificate of Conformity is a significant achievement for Bourns, enabling our valued customers to benefit from the extended lifespan and enhanced reliability of our IsoMOV® protectors across a wider range of designs. The comprehensive documentation required to validate this innovative solution—especially in the absence of an existing IEC standard for hybrid overvoltage protection components—highlights our product team's commitment to delivering top-tier solutions that give our global customers a competitive edge," said Craig Shipley, President of the Bourns Protection Division.

The Bourns® IsoMOV® protector is a fully integrated GDT and MOV hybrid design that combines both devices into a single package, allowing the GDT to block leakage currents through the MOV that may lead to premature failure. It provides an elevated level of surge protection in terms of performance, operational life and enhanced device reliability. Because this compact hybrid design features performance specifications usually found in larger traditional MOV devices, Bourns® IsoMOV® protectors enable designers to better tailor the surge protection performance to their stringent space requirements.

Bourns® IsoMOV® hybrid protectors are available through Bourns’ authorized distribution partners and are RoHS* compliant. For more detailed product information, please see: bourns.com/products/circuit-protection/isomov.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf