MENU
Search
Languages

Bourns Expands Line Filter Line with Series that Features Wide Inductance/Impedance Range and Frequency Up to 300 MHz

Automotive grade, AEC-Q200 compliant Bourns® SRF9005A Series line filters offer high reliability EMI suppression for consumer, industrial and automotive systems

RIVERSIDE, Calif., April 1, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the expansion of its line filter product line with a new series that features a wide inductance and impedance range and frequency up to 300 MHz. Bourns® SRF9005A Series line filters are automotive grade and AEC-Q200 compliant, and are designed to meet critical EMI (Electromagnetic Interference) suppression requirements in a variety of consumer, industrial and automotive systems.

Bourns® new line filters are constructed with a ferrite toroid core, delivering high impedance over a broad frequency range to suppress EMI coming into or leaving the system. They are also excellent common mode power choke solutions for eliminating noise with features that include a current rating up to 1.6 A, an inductance range of 10 to 6500 µH and an operating temperature range of -40 to +105 °C.

The Bourns® SRF9005A Series line filters are available now through Bourns’ authorized distribution partners, and are RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/common-mode-chokes-aec-q200-compliant.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf