Search
Languages

Bourns Announces Two Very High Current Power Inductor Series Designed to Help Improve System Efficiency and Stability

Optimized for industrial high current filters, high current battery charging and DC-DC converters, new power inductors feature shielded construction and low DCR

RIVERSIDE, Calif., March 24, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components power, protection, and sensing solutions, today announced its HRP3822X and HRP5022X Series Shielded Power Inductors. These very high current power inductors feature low DCR and shielded construction for low radiation. Designed to help maintain stable current flow and enhance efficiency in high power applications, Bourns® new shielded power inductors are optimal current management solutions for today’s industrial high current filters, high current battery charging, and DC-DC converters.

In addition, the Bourns® Model HRP3822X and HRP5022X Series have a metal alloy powder core for high saturation current. The series feature an inductance range of 0.68 to 3.3 µH, with DCR from 0.11 to 0.42 mΩ and an operating temperature range of -40 °C to +125 °C.

The Bourns® Series Shielded Power Inductors are available now and is RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/power-inductors-smd-high-current-shielded.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf