Search
Languages

Bourns Expands Digital Current Sensor Line with 500 Amp Series Meeting High Accuracy Measurement Needs in a Wider Range of Applications

The Riedon™ Model SSD-500A Current Sensor – Digital by Bourns offers a precision 24-bit isolated current sensor with CANbus or RS-485 interface options

RIVERSIDE, Calif., December 2, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the release of the Riedon™ Model SSD-500A Series Current Sensor – Digital by Bourns with 500 Amps nominal current. The extended electrical rating allows designers to use a supply voltage of 24 V (15 mA typical), enabling them to meet high accuracy measurement requirements in a wider range of battery-related applications, including large-scale energy storage banks, renewable energy generation infrastructure, industrial motor drives, building automation systems, and EV charging stations.

The Model SSD-500A Series includes advanced digital DC shunt-based current sensors that deliver superior accuracy, stability, and electrical isolation in certain harsh industrial environments. The series also features an internal 24-bit Analog-to-Digital Converter (ADC) that offers plug-and-play simplicity, enabling designers to quickly add high-accuracy current measurement into new designs or retrofit existing ones. These shunt-based sensors also help eliminate the need for periodic device calibrations while also contributing to more efficient use of power. Furthering their design flexibility, the Model SSD-500A Series is offered in RS-485 and CANbus interface options.

The Riedon™ Model SSD-500A Series Current Sensor – Digital by Bourns is available now, and is RoHS* compliant. For additional information, please see: www.bourns.com/products/sensors/current-sensors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf