MENU
Search
Languages

Bourns Announces New Low Profile Line Filter Series that Features a 2.5 mm Profile

Bourns® Model SRF0502 Series line filters provide necessary EMI suppression helping to maximize system uptime in mission-critical applications

RIVERSIDE, Calif., October 28, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced a new low profile line filter series. Featuring a compact 2.5 mm profile, Bourns® Model SRF0502 Series line filters are designed to meet a variety of customer requirements. This new series provides EMI (Electromagnetic Interference) suppression for mission-critical applications where interference must be minimized.

In addition to its low profile design, Bourns® latest line filter series features a shielded construction that further helps to minimize EMI while delivering low DCR, a high current rating up to 5 A and a frequency range up to 700 MHz. These line filters are ideal common mode power choke solutions for eliminating noise in a range of industrial power supplies and other applications that demand high reliability operation.

The Bourns® Model SRF0502 Series line filters are available now and are RoHS* compliant and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/common-mode-chokes.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf