Search
Languages

Bourns Announces New Chip Inductor Series that Offer a High Q Value in a Miniature Size

Model CWF1610 and CWF2414 chip inductors feature wirewound construction to unlock enhanced performance characteristics for RF signal processing and DC power line applications

RIVERSIDE, Calif., August 2, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the CWF1610 and CWF2414 Chip Inductor Series. These inductors employ wirewound construction on a ferrite core to offer high values of inductance, Q values, and self-resonant frequency, plus low DC resistance in a compact size with an operating temperature range of -40 to +125 °C. These features make this series ideal for RF signal processing, resonant circuits, decoupling, noise filters, and DC power line applications for audio headsets, cable modems, set-top boxes, hard disk drives, tablets, and various mobile electronic devices.

Compared to multilayer or film technology, a thicker wirewound construction around the core makes it possible to achieve lower DC resistance and high Q values of 13 to 16 in these miniature-sized inductors. In addition, the high Q values provided in the new inductors -offer designs a high impedance at resonant in inductive-capacitive LC circuits, and low loss at high frequency operation. Bourns® Model CWF1610 and CWF2414 chip inductors also feature a high self-resonant frequency, which translates to low distributed capacitance and maintained inductive characteristics over a wide frequency span. With saturation current up to 860/1100 mA and rated current up to 700/1300 mA, the new chip inductors from Bourns maintain high inductance at a greater peak current matching the requirements in DC power line applications.

Bourns® Model CWF1610 and CWF2414 Chip Inductors are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/chip-inductors-wirewound

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf