Search
Languages

Bourns Announces New Chip Inductor Series that Offer a High Q Value in a Miniature Size

Model CWF1610 and CWF2414 chip inductors feature wirewound construction to unlock enhanced performance characteristics for RF signal processing and DC power line applications

RIVERSIDE, Calif., August 2, 2021 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the CWF1610 and CWF2414 Chip Inductor Series. These inductors employ wirewound construction on a ferrite core to offer high values of inductance, Q values, and self-resonant frequency, plus low DC resistance in a compact size with an operating temperature range of -40 to +125 °C. These features make this series ideal for RF signal processing, resonant circuits, decoupling, noise filters, and DC power line applications for audio headsets, cable modems, set-top boxes, hard disk drives, tablets, and various mobile electronic devices.

Compared to multilayer or film technology, a thicker wirewound construction around the core makes it possible to achieve lower DC resistance and high Q values of 13 to 16 in these miniature-sized inductors. In addition, the high Q values provided in the new inductors -offer designs a high impedance at resonant in inductive-capacitive LC circuits, and low loss at high frequency operation. Bourns® Model CWF1610 and CWF2414 chip inductors also feature a high self-resonant frequency, which translates to low distributed capacitance and maintained inductive characteristics over a wide frequency span. With saturation current up to 860/1100 mA and rated current up to 700/1300 mA, the new chip inductors from Bourns maintain high inductance at a greater peak current matching the requirements in DC power line applications.

Bourns® Model CWF1610 and CWF2414 Chip Inductors are available now and are RoHS compliant* and halogen free**. For more detailed product information, please see: www.bourns.com/products/magnetic-products/chip-inductors-wirewound

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

Über Bourns

Bourns, Inc. ist ein führender Hersteller und Zulieferer von Positions- und Geschwindigkeits-Sensorik, Schutzabschaltungslösungen, magnetischen Komponenten, Mikroelektronikmodulen, Schalttafelsteuerungen und Widerstandsprodukten. Mit Hauptverwaltung in Riverside, Kalifornien beliefert Bourns eine Reihe von Märkten, einschließlich Automobilbranche, Industrie, Haushalt, Kommunikation, nicht-lebenserhaltende medizinische Unterstützungstechnik, Audio sowie viele andere Marktsegmente. Weitere Firmen- und Produktinformationen sind erhältlich auf www.bourns.com.

Bourns® und das Bourns-Emblem sind eingetragene Warenzeichen von Bourns, Inc. und dürfen nur mit Genehmigung von Bourns und nur mit ordnungsgemäßer Anerkennung öffentlich verwendet werden. Andere aufgeführte Namen und Marken sind Warenzeichen oder eingetragene Warenzeichen der jeweiligen Eigentümer.

Agenturkontakt:
Annette Keller
Keller Communication
annettekeller1984@gmail.com
Firmenkontakt:
John McCarthy
Bourns, Inc.
john.mccarthy@bourns.com