Search
Languages

Bourns Announces AEC-Q200 Compliant Current-Compensated Dual Choke Filter Inductor Series with High Current Capabilities

New Model DR334A Line Filters Provide Superior Suppression of Common and Differential Mode Interference in Signal and Power Line Applications

RIVERSIDE, Calif., September 22, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced the Model DR334A Line Filter Series. These current-compensated dual choke filter inductors feature higher current capability than typical standard signal line common mode chokes, as well as high stray inductance and differential mode noise rejection. These capabilities make the Model DR334A series ideal line filter solutions for consumer, industrial and other market power line applications, or in applications where power is transferred over signal lines.

The new Model DR334A series is available in a bifilar-wound configuration to reach higher common mode impedance, and a sector-wound configuration to reach higher differential mode impedance at high frequencies. Offered in a compact, low profile (height 3.6 mm) size and in a broad range of inductance ratings from 11 µH up to 4700 µH, Model DR334A line filters allow designers to set the filter curve best suited to their application.

The Model DR334A series is AEC-Q200 compliant with an extended operating temperature range of –40 to +135 °C and has a rated voltage up to 80 VDC. In addition, the closed and ferrite toroid core construction of Bourns' latest line filter series delivers a more efficient and robust mechanical design.

The Bourns® Model DR334A Line Filter Series is available now, is RoHS* compliant and halogen free**. More detailed product information can be found at: www.bourns.com/products/magnetic-products/common-mode-chokes-aec-q200-compliant/

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf