Search
Languages

Bourns Announces New Sulfur-Resistant Fixed Resistor Series

RIVERSIDE, Calif., June 24, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new sulfur-resistant AEC-Q200 compliant thick film resistor family. The Bourns® Model CRxxxxA-AS chip resistor series is offered in eight different footprints from small 0201 (0603 metric) to 2512 (6432 metric) with rated power from 0.05 to 1 watt. The new surface-mount chip resistors also feature a wide resistance range from 1 ohm to 20 megohms making them ideal for a variety of general-purpose applications.

Bourns designed these resistors to operate in certain harsh environments with higher levels of sulfur contamination. They are manufactured using a thick film element printed onto a ceramic substrate, and tested in accordance with ASTM B809-95 methods, which tests for the porosity of metallic coatings exposed to humid sulfur vapor.

Available now, the Model CRxxxxA-AS chip resistor series complements the other circuit conditioning components from Bourns that include power inductors and rectifier diodes. Bourns' expanded line of sulfur-resistant fixed resistors are RoHS* compliant and halogen free**. For additional product information, please see the datasheet on the Bourns website: www.bourns.com/docs/product-datasheets/crxxxxa-as.pdf.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

***Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf