Leave a message
MENU
Search
Languages

Bourns Introduces Two Compact, Lower Profile TVS Diode Series

RIVERSIDE, Calif., May 8, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced two new TVS diode surge protection series designed to meet the component miniaturization required in today's highly integrated and high power density designs. Bourns® Model SMF4L and Model SMF4L-Q Series are offered in a compact, low profile surface mount SOD-123FL package with a height of just 1.125 mm, which is 50 percent smaller than Bourns' previous generation SMAJ Series TVS diodes.

Bourns optimized these high reliability ESD and voltage transient protection devices for data line, DC power supply and a wide variety of telecom, computer, industrial and consumer electronics applications. Both product series feature standoff voltages of 12 to 58 volts and a peak pulse power dissipation of 400 watts at 10/1000 μs. In addition, Model SMF4L-Q is AEC-Q101 compliant making it well-suited for equipment used in certain more challenging environments.

Bourns® Model SMF4L and SMF4L-Q TVS diodes are available now, and are RoHS compliant*. For more detailed product information: www.bourns.com/products/diodes/tvs-diodes.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
a