Search
Languages

Bourns Announces New AEC-Q101-Compliant TVS Diode Products

RIVERSIDE, Calif., March 18, 2019 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced two new families of AEC-Q101-compliant TVS diode components. Designated Models SM8S-Q and SM8SF-Q, these families are comprised of both unidirectional and bidirectional TVS diodes. They are designed to protect against voltage transients, ESD and EFT surges in DC power supplies and on data lines. Because the new TVS diodes are AEC-Q101-compliant, they are an optimal protection solution for applications that need to meet high reliability requirements such as in equipment that operates in high power, high temperature or in harsh environmental conditions.

Delivering excellent surge performance and offered in a compact DO-218 size package format, the Bourns® Model SM8S-Q Series features a maximum peak power dissipation of 6600 watts. The new Model SM8SF-Q Series offers a high peak pulse power (PPK 10/1000 µs) of 7000 W in ultra-low 1.3mm package profile enabling compact power designs. Customers are able to select from a range of working peak reverse voltages from 16 V up to 43 V for Model SM8S-Q Series, and from 24 V to 36 V with the Model SM8SF-Q Series. Both product families deliver very fast protection with typical response times less than 1.0 picosecond. Furthermore, Bourns’ latest TVS diode components assist compliance to ISO7637-2 and ISO16750-2 surge specifications.

Bourns® Model SM8S-Q and SM8SF-Q Series TVS diodes are available now and are RoHS compliant*. For more detailed product information, please go to: www.bourns.com/products/diodes/diodes-aec-q101-compliant.

* RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf