Search
Languages

Bourns Expands Leading Line of ESD Protection Products with New ChipGuard® Device for Mobile Electronics

RIVERSIDE, Calif., March 13, 2018 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the expansion of its leading line of ESD protection products. The company's new Model CG0201MLC ChipGuard® device delivers ultra-low capacitance (0.2 pF) in a miniature 0201 package. These features meet ongoing performance and small footprint requirements in space-constrained applications such as wearables, handheld devices, headphones, tablets and mobile phones

Bourns designed its latest ChipGuard® device to protect sensitive electronics against electrostatic discharge (ESD) by meeting the IEC 61000-4-2, Level 4 (±8 kV contact/±15 kV air discharge) standard. The Bourns® Model CG0201MLC ChipGuard® device provides fast response of less than one nanosecond to ESD strikes. It also offers bidirectional protection with low clamping voltage, low leakage current and wide operating temperature range.

As a pricing reference, Model CG0201MLC is priced at $0.04 in 15,000 piece quantities. It is available now and is RoHS compliant*. For more detailed product information, please visit: www.bourns.com/products/circuit-protection/chipguard-esd-suppressors.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf