Search
Languages

Bourns Announces High Wattage, Surface Mount TVS Diodes for ESD/EFT/Surge Protection

RIVERSIDE, Calif., September 26, 2016 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new high wattage, surface mount TVS diode series designed for ESD, EFT and surge protection. Bourns' Model 5.0SMDJ TVS diode series answers communications, industrial control and automation, and power supply market needs for increasingly higher power density circuit protection components in more compact packages. The new series supports power wattage up to 5000 watts that helps ensure DC power port and communication lines are well protected against overvoltage transients. They also offer superior line voltage clamping as compared to the performance of competing metal oxide varistor (MOV) technologies.

These unidirectional/bidirectional protection devices feature breakdown voltage from 12 to 170 volts. In addition, Bourns' Model 5.0SMDJ TVS diode series assists compliance with IEC 61000-4-2 ESD (Min. Level 4), IEC 61000-4-4 EFT, and IEC 61000-4-5 Surge industry standards.

Available now, Bourns' Model 5.0SMDJ series is RoHS compliant* and halogen free**. As a pricing reference, Model 5.0SMDJxxA/5.0SMDJxxCA is priced at $0.99 each in 6,000 piece quantities. For more detailed product information, please see the datasheet: www.bourns.com/docs/Product-Datasheets/5-0SMDJ.pdf

*RoHS Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

** Bourns considers a product to be “halogen free” if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf