Search
Languages

Bourns Expands Industry-Leading Current Sense Resistor Product Family

Riverside, Calif., October 29, 2013 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced a new current sense resistor model designed for applications that require lower power, smaller footprint solution. Designated Bourns® model CRF0805, the new device is the smallest surface mount current sense resistor in Bourns' industry-leading CRF family of resistors. Featuring a power rating of just 0.5 watts and a resistance range from 5 milliohms to 20 milliohms, the new model helps meet the ongoing demand for smaller and denser circuit boards. Bourns® fixed resistor products are used to detect and convert current to an easily measured voltage, which is proportional to the current through the device. Current sense resistors offer an optimal solution for designs requiring low inductance and tighter precision for improved reliability and longer life such as power supplies and stepper motor drive applications.

"Our current sense resistors are growing in popularity because of their cost-efficient, high measurement accuracy compared to other device technologies," said Brian Ahearne, Product Line Manager at Bourns, Inc. "The new Bourns® CRF0805 model meets the needs of today's space-constrained, high power density applications. Expanding our current sense resistor line demonstrates Bourns' continued commitment to introduce advanced technologies and solutions that help our OEM customers solve tough design challenges."

The Bourns® CRF0805 model is RoHS compliant* and features an operating temperature range of -55 °C to +170 °C and temperature coefficient of ±100 PPM/°C. Additional specifications are noted in the table below.

Model CRF0805 Technical Specifications

Specification Description
Power Rating @ 70 °C 0.5 W
Derated to Zero Load at +170 °C
Maximum Working Voltage (P x R)1/2
Resistance 0.005 ~ 0.020 Ω
Resistance Tolerance 1 %, ±5 %

Pricing and Availability
As a pricing reference, the Bourns® CRF0805 model is priced from $0.18 in 25,000 piece quantities and is available now. For additional details and specifications, go to www.bourns.com/en/docs/product-datasheets/CRF.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf