Search
Languages

Bourns Adds Three New Application Notes to its Extensive Technical Library

Riverside, Calif., July 24, 2013 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that it has added three new application notes to its extensive technical library. Bourns continually develops new technical resources to help engineers solve design issues and select proven application solutions. The new documents offer development options to maximize LED streetlight reliability, provide an optimal circuit protection design for PoE-based systems and demonstrate the advantages of using non-contacting rotary sensors that help achieve higher reliability in material handling equipment.

Bourns' new application note, "Overcoming Reliability Challenges in LED Streetlight Applications", shows how to address the many reliability challenges, provides a viable solution to open LED failure and presents effective circuit protection options that help increase the application lifespan for LED streetlights in electrically-exposed environments. https://www.bourns.com/en/docs/product-datasheets/Bourns_LED_Streetlighting_AppNote.pdf

A new application note, "Enhancing the Operational Reliability of Material Handling Equipment", provides valuable design information that allows developers to upgrade and extend the life of material handling equipment such as forklifts, pallet jacks, scissor lifts and other types of robotic machinery. The note highlights the use of non-contacting rotary sensors as a viable technology solution to overcome many of the design limitations of contacting technology components and optical encoders. https://www.bourns.com/en/docs/product-datasheets/Bourns_AMS22_Material_Handling_AppNote.pdf

Presenting a robust lightning protection circuit solution for PoE-based applications, Bourns' third new application note is entitled, "Lightning Surge and AC Power Cross Protection for PoE Applications." This valuable design resource highlights a new solution where the protection circuit is capable of withstanding severe lightning surges such as 4 kV 10/700 μs voltage surges per ITU-T K.44. It also explains how to implement effective AC power cross protection and demonstrates how this solution has minimal impact on signal integrity in low voltage, high-speed communication circuits. https://www.bourns.com/en/docs/product-datasheets/Bourns_Lightning_Surge_Prot_PoE_TCS_AppNote.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf