MENU
Search
Languages

New Models Designed to Help Increase Product Life and Provide High Reliability for Applications Operating in Rugged Environments

Riverside, Calif., February 19, 2013 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced it has expanded its line of non-contacting rotary position sensors with two new models. Designed to help increase the product lifespan and reliability of applications that operate in rugged environments, the Bourns® Model AMS22U and Model AMM20B utilize magnetic Hall Effect (HE) technology that helps increase operational life and reliability even in harsh environments. Bourns® non-contacting rotary position sensors offer an ideal solution for applications such as patient platform position feedback, pneumatic control valve position feedback, actuator motor position feedback, lift/shuttle suspension systems, and tilt control feedback. These applications are used in a wide range of industrial, commercial, medical, and automotive applications.

"In response to evolving requirements for higher performance and product longevity for applications that must operate in harsh or rugged environments, Bourns' new non-contacting position sensors offer a cost-effective solution that meets stringent reliability standards," said Chuck Manzano, Application Engineer for Sensors and Controls at Bourns, Inc. "In addition, our customers are finding non-contacting sensing technology much more attractive due to its consistent performance over life and excellent performance in harsh environments resulting in reduced component replacement costs."

The Bourns® Model AMS22U is a single-turn, non-contacting rotary position sensor that offers a rotational life of up to 100 million cycles for superior longevity and reliability. The new sensor features a 1/8-inch shaft supported by dual ball bearings and a factory programmable electrical angle from 10 to 360 degrees.

The Bourns® Model AMM20B is a multiturn, non-contacting rotary position sensor that features a rotational life of up to 50 million cycles, depending on the product and particular application. The new sensor features a slim profile package for space constrained applications, 12-bit resolution and a factory programmable electrical angle from 1080 to 3600 degrees.

Pricing and Availability
The new non-contacting rotary position sensors are available now in samples and production quantities. As a pricing reference, the Bourns® Model AMS22U is priced at $35 each in 1,000 piece quantities. The Bourns® Model AMM20B is priced at $24 each in 1,000 piece quantities. Both models are available through Bourns' distribution sales channels.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf