Search
Languages

Bourns Announces its Lowest Resistance Battery Strap Resettable Fuse

Riverside, Calif., April 27, 2011 — Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the company's smallest battery strap resettable fuse featuring ultra-low resistance designed to deliver reliable and robust circuit protection. Designated the Bourns® Multifuse® MF-LL Series, the new battery strap resettable fuse was developed in response to portable electronics industry demand for a miniature-sized, resettable overcurrent protection with the lowest possible resistance. The new fuse meets the circuit protection requirements of rechargeable battery packs used in portable electronic devices such as mobile phones, MP3 players and digital cameras.

"Using its lowest resistance PTC formulation to date, Bourns has produced a resettable fuse from a chip of less than 11 mm2. Resettable fuses of such small size generally have quite high resistance values, but Bourns' new MF-LL Series overcomes this limitation and offers an initial resistance of just 5 to 15 mOhms," said Brian Ahearne, Multifuse® product line manager at Bourns, Inc. "As the electronics industry continues to evolve at a rapid pace, the launch of the new MF-LL Series demonstrates Bourns' ongoing commitment to next-generation resettable fuse development."

The Bourns® MF-LL1190 Model is available now. Future models in the series are in development and are scheduled for release in the second quarter of 2011. The MF-LL Series is also RoHS* compliant. As a pricing example, Bourns® MF-LL190 is priced at $0.25 each in 10K piece quantities.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf