MENU
Search
Languages

Bourns Announces New Circuit Protection TBU® Series that Features a Broad Range of Trigger Currents and Voltages

Riverside, Calif., September 7, 2010 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the company's next-generation Transient Blocking Unit (TBU®) Series of circuit protection devices designed to protect a broad selection of industrial and telecommunications applications. The new series provides ultra-fast overcurrent protection offered in a wide range of trigger currents and voltages and reduced form factors to save valuable board space. Designated the Bourns® TBU-CA Series, the new devices are electronic current limiters (ECL) that are triggered by excessive voltage or current. Designed as an optimal circuit protection solution for industrial controls, medical electronics, automated test systems, and military and aerospace applications, the Bourns® TBU-CA Series can be used for protection on Ethernet, RS-485, HART and other ports where dangerous surge and power cross events may occur. The circuit protection device series can also be used in telecom applications and provides a barrier to surges while allowing high frequency signals such as VDSL2 to pass through without damage to the circuit.

Protecting sensitive electronics and applications from the potentially damaging effects of surges that can cause current and voltage to rise above normal operating levels, the Bourns® TBU-CA Series eliminates the need for large shunt protection devices by stopping the damaging currents from reaching protected circuits in less than one microsecond. The new circuit protection devices are low capacitance, single bidirectional high speed devices designed to protect against faults caused by short circuits, AC power cross, induction and lightning surges within rated limits. The resettable devices also feature significantly lower let-thru energy and overshoot protection, which reduces stress on the printed circuit board (PCB) for increased reliability and product life.

"Higher data rates combined with more sensitive electronics presents a real challenge for protection engineers," said Paul Wiener, telecom market director at Bourns. "Bourns' unique TBU® protection technology limits the energy allowed into sensitive electronics without loading high data rate lines with capacitance. This allows designers to place high performance protection on even their highest bandwidth applications. "

The Bourns® TBU-CA Series is available in five impulse blocking voltages from 250V to 850V with minimum trip currents of 50 mA to 500 mA featuring resistance values as low as 3 ohms. Product samples, evaluation boards and sample kits are available now through Bourns' distribution partners. As a pricing example, Bourns® TBU-CA085-500-WH is priced at ($.69 each) in (10K) quantities.

About Bourns® TBU® Technology
Bourns' TBU® High Speed Protector is the first new approach to electronics circuit protection in over a decade. This technology is designed to block a transient through a current disconnecting mechanism. Rather than a complex interstage coordination between two shunting components, the TBU® device allows customers to protect circuit boards from both overvoltage and overcurrent surges. The TBU® device protects electronic equipment within nanoseconds, essentially eliminating latency common in the circuit protection design, limiting let-through energy. The TBU® device has virtually no capacitance or inductance, and therefore can be used in high bandwidth applications. It has a resistive characteristic which permits currents up to a certain level to pass unimpeded to the protected interface. In higher current situations, the TBU® device switches to a high impedance state, protecting until the surge voltage dissipates or the short-circuit reseals. The TBU® device offers full bi-directional operation, which is inherently resettable.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
a