Search
Languages

伝説的なギターリストでソングライターの Jeff Carlisi、2010 年夏季 NAMM ショーの Bourns ブースに登場

Riverside, Calif., June 1, 2010 — Bourns, Inc. today announced that Jeff Carlisi, former guitarist of the rock band 38 Special, will make an appearance in Bourns’ booth during the upcoming Summer NAMM Show, June 18-20, 2010 in Nashville, Tenn. Carlisi will meet attendees and sign autographs to help promote Bourns’ industry-leading line of guitar potentiometers. The legendary guitarist/songwriter will also be promoting CAMP JAM, his summer rock music camp for kids and teens.

Attendees of the Summer NAMM Show are invited to meet Jeff Carlisi.

Where: Bourns’ booth #1245
When: Friday, June 18: 2:30 – 3:30 PM
Saturday, June 19: 11:00 AM – 12:00 PM


Carlisi has used Bourns’ guitar potentiometers for more than 30 years and is a supporter of the company’s products. As the original guitarist and songwriter for the classic southern rock band 38 Special, Carlisi has five platinum albums that include mega-hit songs “Caught Up in You,” “Second Chance,” and “Hold on Loosely.” Today, Carlisi is helping young aspiring musicians make their rock star dreams come true with CAMP JAM, which he co-founded in 2004.

CAMP JAM is the ultimate summer rock music camp for kids and teens and is held in 17 cities across the U.S. and Canada. The CAMP JAM program gives young musicians the chance to meet others their age for the rock ‘n’ roll experience of a lifetime—from forming their own bands and playing a concert to hanging out with rock music legends. For more information, visit www.campjam.com.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf