Search
Languages

Bourns Announces freeXpansion™ Technology for its Multifuse® Polymer PTC Resettable Fuses

RIVERSIDE, Calif., March 23, 2009

Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that the company has developed freeXpansion™, a new technology added to the company’s entire line of Multifuse® surface mount polymer positive temperature coefficient (PTC) resettable fuses. This new technology increases the performance of the fuse with the ability to handle higher currents and voltages, improves its resistance stability and allows for a smaller footprint. Due to its new freeXpansion technology, Bourns is able to introduce one of the smallest families of PTCs on the market with a size of 0603, designated the Bourns MF-FSMF Series. Bourns’ Multifuse surface mount devices manufactured using the freeXpansion process is designed to meet next-generation electronics smaller size and high current requirements. Multifuse devices are an optimal overcurrent circuit protection solution for broad range of equipment including products with USB 2.0, USB 3.0 and HDMI ports and in consumer electronics and automotive electronics applications.

Polymer PTC resettable fuses expand when an overcurrent event occurs and contracts when they reset. The freeXpansion technology allows the device to freely expand and contract without mechanical restrictions for more stable performance, extended product life and to be manufactured in a smaller size.

&;quot;Bourns Multifuse products with freeXpansion offer distinct competitive advantages for our customers enabling reliable circuit protection across a broader range of applications,” said Brian Ahearne, technical marketing manager for Bourns’ Multifuse products. “As more and more electronic products become portable with design space constraints, Bourns Multifuse devices match application requirements for a smaller package and the ability to handle higher currents and voltages helping our OEM customers protect their valuable circuits from overcurrent conditions.”

Bourns Multifuse devices act as critical circuit protection components by limiting dangerous current surges, such as short circuits in electrical equipment. These devices provide secure protection as they react to an over-current event by changing from a very low resistive state to a very high resistive state. This is also referred to as the positive temperature coefficient effect or PTC effect. Once the overcurrent surge has passed, the Multifuse device automatically resets to its low resistive state and allows the equipment to resume operation.

Pricing and Availability
Bourns’ line of surface mount Multifuse devices with new freeXpansion technology is available now. For complete model numbers and sizes, go to Bourns’ site at www.bourns.com/multifuse. As a pricing reference, devices with freeXpansion are priced from $0.25-$0.35 in 6,000 piece quantities.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf