Search
Languages

Bourns Releases PoE-LAB1 Design Kit to Help Streamline Power/Data Delivery and Protection Designs in Power over Ethernet Applications

RIVERSIDE, Calif., June 11, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced the release of its highly functional POE-LAB1 Design Kit, created to help streamline both the designing of power/data delivery and protection in Power over Ethernet (PoE) applications. The kit includes advanced components from Bourns’ broad portfolio of Semiconductor and Magnetic products that are particularly suited to support high-speed Ethernet lines (up to 10 GbE) with PoE++ (Type 4) capabilities.

A Bourns first, this kit provides a synergistic approach that gives developers a useful resource with a wide range of options for their PoE designs that can satisfy a variety of power/data delivery and protection requirements. The Bourns® POE-LAB1 Design Kit comes with 32 different products. This allows designers to evaluate how multiple product combinations can meet various PoE application specifications, all using a convenient single design kit. The Bourns® products in the kit are comprised of Ethernet transformers, DC-DC conversion transformers, a common mode choke, ferrite beads, single and bridge Schottky rectifier diodes, Bourns® TBU® and TCS™ high-speed protectors, diode arrays and TVS diodes.

The Bourns® PoE-LAB1 Design Kit is available now. For additional information, please see: www.bourns.com/resources/design-tools/design-kits/magnetics#poelab1.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com