Leave a message
MENU
Search
Languages

Bourns Introduces High Clearance / Creepage Distance Isolation Power Transformer Series

RIVERSIDE, Calif., February 19, 2020 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its new high clearance/creepage distance isolation power transformer series. Bourns® Model HCT series high-voltage isolation push-pull transformers are AEC-Q200 compliant. Bourns designed its latest transformer series to support isolated interface power for CAN, RS-485, RS-422, RS-232, SPI, I2C, and lower-power LAN. Solutions that simplify isolated interface power are required in a broad range of applications including those designed to meet Industry 4.0 and in low/medium risk medical** sensors, communication PHYs and metering. The capabilities of the Bourns® Model HCT series are also ideal solutions for circuits requiring low DC power and any application where isolation from potentially hazardous voltages are needed such as from a high-voltage battery.

The Bourns® Model HCT series features an input range of 3.3 to 5 V and delivers 3.3 to 15 V and up to 350 mA output, configured in a variety of turns ratios. The new series is constructed with a ferrite toroid core for high coupling factor and efficiency. Furthermore, the new power transformers are offered in a low-profile 6.5 mm housing with reinforced insulation, at least 8 mm clearance / creepage distance and 4.2kVac withstanding voltage to provide an elevated degree of isolation from high voltage hazards.

Designed for isolation power supplies using Texas Instruments SN6501 and SN6505B transformer drivers, HCT series transformers are compatible with spread spectrum modulation for reduced emissions, and are compliant with IEC 60950-1, IEC 62368-1, IEC 60664-1 and AEC-Q200 standards.

Available now, the Bourns® HCT high-voltage power transformer series is RoHS** compliant. For additional product information, please see: www.bourns.com/products/magnetic-products/transformers-power

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns® products have not been designed for and are not intended for use in "lifesaving," "life-critical" or "life-sustaining" applications nor any other applications where failure or malfunction of the Bourns® product may result in personal injury or death. See Legal Disclaimer Notice www.bourns.com/docs/legal/disclaimer.pdf

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
a