Leave a message
MENU
Search
Languages

Bourns Expands the Series of Useful Design Documentation on Port Interface Circuit Protection

Riverside, Calif., March 29, 2011 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that it has developed seven new PortNote™ Solutions to assist designers in selecting the appropriate circuit protection solution for a specific port interface. Bourns® PortNote™ Solutions are a series of one-page documents that provide concise information on relevant compliance standards, Bourns solutions and part numbers, the specific interface schematic and alternative solution references. The new documents also feature application-based tools for audio/video and data communication and telecommunications designs, and are a useful resource to help streamline the circuit protection selection process for a specific port interface.

"Selecting the right circuit protection solution for a particular port interface can be time consuming and daunting," said Dr. Erik Meijer, vice president of circuit protection at Bourns. "With our extensive circuit protection knowledge, Bourns is committed to helping our customers reduce their development time. Because our unique PortNote™ Solutions documentation has been positively received, we have chosen to add seven more popular port solutions to this successful series."
 
Easily accessible on the Bourns website, the seven new PortNote™ Solutions cover Ethernet and RS-485 ports for datacom applications; LVDS input and output ports for audio/video applications and T1/E1 telephony, VDSL line side and VDSL over POTs for ports in telecom designs. In addition, Bourns offers corresponding design kits. Each design kit contains sufficient Bourns® products to build five of the circuits offered in the PortNote™ Solution. Bourns® PortNote™ Solutions are not intended to replace detailed application notes or the customized solutions provided by Bourns' FAE teams, but instead provide useful information in the circuit protection selection process for a specific port interface. A total of 22 individual Bourns® PortNote™ Solutions including the corresponding design kits can be viewed on the Bourns website at www.bourns.com/Library.aspx?name=PortNoteSolutions.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
a