MENU
Search
Languages

Bourns Announces New Multiturn Precision Potentiometer Slip Clutch Option

Riverside, Calif., November 10, 2010 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced that the company is now offering a new "slip clutch" option in specific multiturn potentiometers models. The slip clutch developed by Bourns for its Models 3547, 3548 and 3549 is designed as a safety feature that helps prevent damage to the potentiometer in applications where the full travel is used thereby increasing reliability and reducing potential service costs and system downtime. Bourns' multiturn potentiometers with the slip clutch are an optimal solution in mechanized or machine-to-machine applications such as linear actuators, cable transducers and mechanical position sensors where the mechanical actuator may occasionally rotate the shaft beyond the mechanical stops, or beyond the set number of turns.

Bourns® multiturn potentiometer slip clutch option is an internal design feature that does not alter the physical dimensions of the component. This new feature allows the device to idle at the extreme clockwise or counter-clockwise ends without inducing damage to the stops on the potentiometer.

"This unique and useful new feature was developed in response to requests from our industrial, medical and aerospace customers that have the requirement to protect multiturn potentiometers in the event that equipment goes out of calibration," said Chuck Manzano, product manager at Bourns, Inc. "Bourns is the first to market with this new option and highlights our commitment to product innovation and continuous improvement based on customer feedback. This new option will provide our customers with a more reliable solution in mechanized applications, while providing our customers with added value."

As a pricing reference, the Model 3547 3-turn and Model 3548 5-turn precision potentiometer with slip clutch option is priced at $16.99-$18.31 in 1,000 piece quantities. The Model 3549 10-turn precision potentiometer with slip clutch option is priced at $14.44-$15.49 in 1,000 piece quantities. Hybritron® versions are also available at higher prices. Samples and production quantities of all three models with the new slip clutch option are available now.

Bourns® and the Bourns logo are registered trademarks of Bourns, Inc. and may be used only with the permission of Bourns and proper acknowledgement. Other listed names and brands are trademarks or registered trademarks of their respective owners.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com
a