Search
Languages

Bourns Adds Highly Reliable, Long Rotational Life Rotary Position Sensor to its Trimpot Product Line

RIVERSIDE, Calif, September 9, 2008 — Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of a new 12 millimeter (mm) rotary position sensor. The small and highly reliable new dust-proof rotary sensor, designated Model 3382, provides long product life with its 1 million rotational cycles and IP40 seal rating. The Bourns Model 3382 is the latest addition to the company’s Trimpot product line and is designed for a wide range of space-constrained applications requiring high quality and reliability such as navigation systems, automotive power seats and mirrors, portable electronic equipment, digital cameras, industrial equipment and controls, robotic systems and home applications including mechanical compartment systems, appliances, in-wall temperature control systems and more.

“Bourns’ new rotary position sensor offers a more economical and reliable solution for many applications compared to conventional panel controls,” said Emill Melliz, Trimpot product line manager at Bourns. “The low profile, simple and elegant design gives our customers greater design flexibility, and Bourns will  extend that design flexibility with new configurations and options that will be available in the near future.”

Bourns’ Model 3382 rotary position sensor has a shaftless, surface-mount design that features exceptional performance characteristics including a broad operating temperature range (-40ºC to +120ºC), and great independent linearity (+2%) for its compact size. This device is well suited for applications that require frequent adjustment where it is necessary to control a variable output such as frequency, speed, contrast, brightness intensity, or volume control. The design is also a good solution for applications where a mechanical angular displacement is measured by the device’s proportional ouput signal. 

Pricing and Availability
Bourns’ Model 3382 12mm dust-proof rotary position sensor is available now in production quantities. As a pricing reference, the Model 3382 is offered in the price range of $1.10 to $1.20 for 1,000 piece quantities through distribution.

关于美国柏恩(Bourns)

Bourns — 是电子零组件业界的龙头制造供货商,公司总部位于美国加州的河边市,其产品包含:位置与速度传感器、电路保护解决方案、磁性组件、微电子模块、面板控制器及电阻产品,服务产业涵盖汽车、工业、消费、通信、非关键性的生命支持医疗(低/中风险)、音频以及其他各种市场。如需了解更多的公司与产品讯息,欢迎上公司网站查询:www.bourns.com