Search
Languages

美国柏恩(Bourns)推出新ChipGuard®汽车ESD保护器件

河边市, 加州, Dec 17, 2013 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the introduction of new ChipGuard® ESD protectors designed specifically to guard sensitive automotive electronics from the threat of electrostatic discharge (ESD) and are qualified to meet up to IEC 61000-4-2 Level 4 standards. Designated the Bourns® CGA-MLC Series of ESD protectors, these extremely fast bidirectional devices have low capacitance, minimal insertion loss and low leakage over a wide temperature range. The new devices from Bourns are available in ultra-small, industry standard 0402 and 0603 packages. The Bourns ChipGuard® MLC Series of ESD protectors are an ideal protection solution for a large range of automotive applications including antenna circuits, camera links, sensors, touchscreen interfaces, GPS systems, USB 3.0 devices and high-speed communication buses.

"Answering the needs of our automotive customers, Bourns expressly designed our new MLC Series of ESD protectors to deliver the high performance and reliability required for today's sensitive automotive applications," said Kurt Wattelet, Communications Division at Bourns, Inc. "Bourns continually strives to introduce products that our customers need to excel in their respective industries, and this new series of ESD protectors provides the advanced technology needed for the broad spectrum of high speed digital electronics employed in vehicles today."

The Bourns® ChipGuard® MLC Series are fast-response protectors, designed to withstand multi-strike ESD threats, are RoHS* compliant and are fully AEC-Q200 qualified and supported.

Pricing and Availability
The Bourns® CGA-MLC Series of ESD protectors are available now. As a pricing reference, an ESD protector in a 0402 package is priced at $0.08 each in 30,000 piece quantities. For additional product information and specifications, please go to: www.bourns.com/docs/product-datasheets/CGA-MLC.pdf.

*RoHs Directive 2002/95/EC Jan. 27, 2003 including annex and RoHS Recast 2011/65/EU June 8, 2011.

关于 Bourns

Bourns — 是一家私人控股制造商,专注于电力电子、电阻组件、电路保护及传感解决方案。公司成立于 1947 年,总部位于美国加州河边市 (Riverside, California),透过全球设计、制造与销售网络,服务汽车、工业、消费性电子、通信、医疗 与音频市场。如需了解更多的公司与产品信息,欢迎上公司网站查询:www.bourns.com