Search
Languages

美国柏恩(Bourns)发布新款10/100 Base-Tx 变压器 MB及ADSL调制解调器最佳电感组件解决方案

河边市, 加州, Jun 10, 2014 - Bourns, Inc., a leading manufacturer and supplier of electronic components, today introduced its new 10/100 Base-Tx Transformer. Designated the Bourns® Model PT61018PEL, it is an addition to the company's comprehensive inductive components product family. This LAN transformer features a single-port, small size, potted construction design that makes it an optimal solution for Ethernet MB and ADSL-based modems. Bourns' new LAN 10/100 Base-Tx transformer is also ideal for harsh environment applications offering extended temperature range (-40 to +85 °C) operation with 1.5K Vrms isolation voltage. The PT61018PEL can be used as alternate transformer to Bourns' existing Model PT61018EL, and offers a significantly shorter production lead time of 10 weeks compared to the existing model.

"Bourns' new LAN 10/100 Base-TX transformer is a welcome addition to our broad array of magnetic components and solutions that meet a variety of application needs," said Guido Zehnder, product manager at Bourns, Inc. "In addition to its ruggedized potted construction design and extended temperature operation that meet harsh environment modem application requirements, Bourns' latest LAN transformer is fully integrated for adapter, hub and motherboard applications."

Pricing and Availability As a pricing reference, the Bourns® model PT61018PEL is priced at $0.60 each in 5000 piece quantities. Available immediately, the new LAN transformer is IEEE 802.3 Ethernet compatible, is offered in a dual channel 16-pin SMD package and is RoHS compliant*. For additional product specifications, please go to: www.bourns.com/docs/product-datasheets/PT61018PEL.pdf

关于 Bourns

Bourns — 是一家私人控股制造商,专注于电力电子、电阻组件、电路保护及传感解决方案。公司成立于 1947 年,总部位于美国加州河边市 (Riverside, California),透过全球设计、制造与销售网络,服务汽车、工业、消费性电子、通信、医疗 与音频市场。如需了解更多的公司与产品信息,欢迎上公司网站查询:www.bourns.com