MENU
Search
Languages

Bourns Announces New Low Capacitance TISP Surge Protectors Optimized for ADSL and VDSL Applications

Riverside, Calif., January 27, 2009 Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of a new family of low capacitance surge protectors designed to protect ADSL, ADSL2, ADSL2+, VDSL and VDSL2 ports in modems or telephone exchanges. Designated the TISP4C015L1N, TISP4C020L1N and TISP4C025L1N, Bourns’ new family of surge protectors have a small footprint and are designed to reduce line failure and help to increase xDSL line reach to customers with a low capacitance of 9 picofarads (pF) and a feed-through package that is designed to provide the lowest possible protection voltage. This new family of Thyristor Surge Protection Devices (TSPD) is based on Bourns industry-leading TISP® overvoltage protection technology that follows in the company's history of providing leading-edge and cost effective solutions and recommendations.

“Bourns’ new family of TISP surge protectors is an ideal solution for modems or telephone exchange ports due to its small size, feed-through package and ultra low capacitance,” said Koenraad Rutgers, technical marketing manager at Bourns. “We already have design wins from our OEM customers based on our product performance that provide solutions to help reduce line failures and maximize xDSL line reach.”

As the VDSL market continues to grow with more than 100 million lines installed in 2008 alone, Bourns’ new family of surge protector products is designed to protect xDSL line-driver interfaces at both ends of the line from overvoltages from AC power system or lightning-flash disturbances. These symmetrical protectors are two-terminal thyristor-crowbar devices and can be used to protect between conductors, or a pair of devices can be deployed to protect from line to ground. When placed between the xDSL line driver IC and the transformer, this protector will clamp and switch into a low-impedance state, safely diverting the energy transferred by the xDSL coupling transformer. The low capacitance design makes these devices an optimal choice for designs from ADSL all the way up to 30 MHz VDSL2. The alternative to TISP surge protectors had previously been simple steering diodes which allow energy to reach the protected line drivers, potentially resulting in line damage.   

Pricing and Availability
Bourns’ TISP4CO15L1N, TISP4CO20L1N and TISP4C025L1N surge protectors are available now. As a pricing reference, the TISP4 surge protector products are offered at $0.20 in 1 million-unit quantities through distribution.

关于美国柏恩(Bourns)

Bourns — 是电子零组件业界的龙头制造供货商,公司总部位于美国加州的河边市,其产品包含:位置与速度传感器、电路保护解决方案、磁性组件、微电子模块、面板控制器及电阻产品,服务产业涵盖汽车、工业、消费、通信、非关键性的生命支持医疗(低/中风险)、音频以及其他各种市场。如需了解更多的公司与产品讯息,欢迎上公司网站查询:www.bourns.com