Search
Languages

Bourns Adds Highly Reliable, Long Rotational Life Rotary Position Sensor to its Trimpot Product Line

RIVERSIDE, Calif, September 9, 2008 — Bourns, Inc., a leading manufacturer and supplier of electronic components, today announced the availability of a new 12 millimeter (mm) rotary position sensor. The small and highly reliable new dust-proof rotary sensor, designated Model 3382, provides long product life with its 1 million rotational cycles and IP40 seal rating. The Bourns Model 3382 is the latest addition to the company’s Trimpot product line and is designed for a wide range of space-constrained applications requiring high quality and reliability such as navigation systems, automotive power seats and mirrors, portable electronic equipment, digital cameras, industrial equipment and controls, robotic systems and home applications including mechanical compartment systems, appliances, in-wall temperature control systems and more.

“Bourns’ new rotary position sensor offers a more economical and reliable solution for many applications compared to conventional panel controls,” said Emill Melliz, Trimpot product line manager at Bourns. “The low profile, simple and elegant design gives our customers greater design flexibility, and Bourns will  extend that design flexibility with new configurations and options that will be available in the near future.”

Bourns’ Model 3382 rotary position sensor has a shaftless, surface-mount design that features exceptional performance characteristics including a broad operating temperature range (-40ºC to +120ºC), and great independent linearity (+2%) for its compact size. This device is well suited for applications that require frequent adjustment where it is necessary to control a variable output such as frequency, speed, contrast, brightness intensity, or volume control. The design is also a good solution for applications where a mechanical angular displacement is measured by the device’s proportional ouput signal. 

Pricing and Availability
Bourns’ Model 3382 12mm dust-proof rotary position sensor is available now in production quantities. As a pricing reference, the Model 3382 is offered in the price range of $1.10 to $1.20 for 1,000 piece quantities through distribution.

关于 Bourns

Bourns — 是一家私人控股制造商,专注于电力电子、电阻组件、电路保护及传感解决方案。公司成立于 1947 年,总部位于美国加州河边市 (Riverside, California),透过全球设计、制造与销售网络,服务汽车、工业、消费性电子、通信、医疗 与音频市场。如需了解更多的公司与产品信息,欢迎上公司网站查询:www.bourns.com