Search
Languages

Bourns Unveils Current Transformer Line with New Model that Features High Turns Ratio with Permalloy T-Core Construction

Bourns® Model PCP300-T414250S Current Transformer provides high permeability and low energy losses delivering excellent high frequency current sensing for power systems

RIVERSIDE, Calif., June 2, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today unveiled the Company’s new current transformer line with its Model PCP300-T414250S Transformer. The new model is made with high-efficiency permalloy material that helps reduce heat loss and energy consumption. This technology also enables fast power conversion rates with elevated precision, making this transformer ideal for power quality analysis. In addition, its advanced features support a wide range of rated current measurements, including high-frequency current sensing in power meters and motor load monitoring.

The Model PCP300-T414250S Current Transformer has a maximum primary continuous current of 300 A, with a dielectric strength of up to 3.5 kV, which are required to help ensure the safety of both equipment and personnel. Additionally, the new transformer features a protective coil housing design suitable for applications that operate in challenging environments. Bourns designed this new current transformer line to allow customers to achieve faster, higher stability and safe electricity monitoring and management.

The Bourns® Model PCP300-T414250S current transformer is available now through Bourns’ authorized distribution partners, and is RoHS* compliant and halogen free**. For more detailed product information, please see: bourns.com/products/magnetic-products/current-transformers.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

**Bourns considers a product to be "halogen free" if (a) the Bromine (Br) content is 900 ppm or less; (b) the Chlorine (Cl) content is 900 ppm or less; and (c) the total Bromine (Br) and Chlorine (Cl) content is 1500 ppm or less.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf