Search
Languages

Bourns Broadens Environmental Sensor Line with New Analog and Digital Pressure Sensors with Extensive PSI Range

The Bourns® BPS160 Series and BPS170 Series provide superior performance in ultra-low pressure sensing applications and additional digital system design flexibility

RIVERSIDE, Calif., March 31, 2025 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced that is has broadened its environmental sensor product line with two new pressure sensor series. The Bourns® BPS160 Series Analog Pressure Sensors and the BPS170 Series Digital Pressure Sensors are designed to provide superior performance in ultra-low pressure sensing applications. Both series deliver an extensive (-14.5 to 14.5) PSI range that makes them suitable to a wider variety of applications that include medium/low risk† medical equipment, white goods, industrial P/I and process control systems.

Available in a compact, surface mount package, the two pressure sensors series enable design flexibility for use in digital systems, and also offer compensated plug and play that helps to reduce development time. Designed with dual horizontal ports, 13-bit Digital-to- Analog Conversion (DAC) resolution and an operating temperature range of -20 ºC to 100 ºC, Bourns latest gauge sensors deliver excellent linearity for consistent measurement across various environmental conditions.

Both the Bourns® BPS160 Series analog pressure sensors and BPS170 Series digital pressure sensors are available now and are RoHS* compliant. For more detailed product information, please see: bourns.com/products/sensors/environmental-sensors/compensated-pressure-sensors.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf