Search
Languages

Bourns Releases Current Sensor Series that Features High Accuracy with Superior Operational Stability

The Riedon™ Model SSA-2 Current Sensor – Analog by Bourns provides immunity to stray magnetic fields and meets unipolar power supply requirements

RIVERSIDE, Calif., December 2, 2024 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today released its Riedon™ Model SSA-2 Series Current Sensor – Analog by Bourns. These shunt sensors deliver a high accuracy current sensing solution with greater operational stability compared to typical Hall effect sensors. This series is designed to provide immunity to stray magnetic fields as they can detrimentally interfere with the operation of sensors in sensitive electronic devices, potentially causing inaccurate readings, device failure or even safety hazards. In addition, the Model SSA-2 Series meets unipolar power supply requirements, making these devices superior measurement choices for a wide variety of battery-related current sensing applications including large-scale energy storage banks, renewable energy generation infrastructure, industrial motor drives, building automation systems, and fuel cells.

The Model SSA-2 Series includes innovatively designed analog technology that could offer higher performance than Hall Effect technology, with ±0.1 % sensing accuracy and ±0.1 % linearity over their entire current range, with low susceptibility to temperature drift. In addition, the sensors’ low-noise resolution and offset performance allows accurate low-current measurements, and also provides excellent gain and linearity performance over the entire temperature range. Offering wide bandwidth AC and DC support, this series features nominal current range values from 100 A to 1000 A, making it more adaptable to different environments and a wide variety of market applications.

The Riedon™ Model SSA-2 Series Current Sensor – Analog by Bourns is available now, and is RoHS* compliant. For additional information, please see: www.bourns.com/products/sensors/current-sensors.

About Bourns

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf