Search
Languages

Bourns Unveils its Smallest Automatically Resettable Surface Mount Mini-breaker Device

Model SW Miniature Thermal Cutoff (TCO) device is designed to provide lower current application overtemperature protection and can be used as an overtemperature sensor

RIVERSIDE, Calif., November 8, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced its smallest surface mount mini-breaker TCO device. The Bourns® Model SW mini-breaker has a 4.7 mm x 2.8 mm footprint with a height of just 0.94 mm. Designed to control abnormal, excessive temperature virtually instantaneously, up to rated limits, the Model SW mini-breaker is an optimal overtemperature protection solution for a wide range of applications that include LED systems, wireless charging coils, motors, and for a variety of printed circuit board components. This new model mini-breaker can also be used as an overtemperature sensor.

The new Model SW mini-breaker complements Bourns' latest Model SD Series with features and functionality that meet lower current protection application requirements. It offers a trip temperature setting of 70 °C ±5 °C, with maximum resistance values of 5 mΩ. For wireless charging applications, this mini-breaker model can operate up to 100 V peak (AC 128 kHz). Manufactured using Bourns' highest rated corrosion resistant bimetal mechanism, this mini-breaker model is also designed to withstand humid environments.

Bourns® Model SW mini-breaker device is available now and is RoHS* compliant. For detailed product information, please see: www.bourns.com/products/mini-breakers.

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.) は、位置センサー、速度センサー、回路保護ソリューション、磁気部品、マイクロ電子モジュール、パネル制御部品、抵抗部品の一流メーカーであり、サプライヤーでもあります。米国カリフォルニア州リバーサイドに本社を置く Bourns は、自動車、産業、消費者、通信、ノンクリティカルなライフサポート医療、オーディオをはじめとする多様な市場セグメントにおいて活動しています。当社および製品に関する詳しい情報は、www.bourns.com をご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf

メディアエージェンシー窓口:
Annette Keller
Keller Communication
(949) 947-7232
annettekeller1984@gmail.com
弊社窓口:
Josephine Chen
Bourns Asia Pacific, Inc.
886-2-2562-4117 #138
Josephine.chen@bourns.com