Search
Languages

Bourns Introduces High Voltage 2-Electrode GDT Series Designed for IEC 62368-1 Compliant Equipment and Powerline Protection

The Bourns® Model GDT28H Series features high insulation resistance and an enhanced surge rate in a compact 8 mm form factor; ideal for AC line applications

RIVERSIDE, Calif., August 8, 2023 - Bourns, Inc., a leading manufacturer and supplier of electronic components for power, protection, and sensing solutions, today announced an addition to its next-generation gas discharge tube (GDT) product line with the introduction of a high voltage 2-electrode overvoltage protector family. The Bourns® Model GDT28H Series is designed to meet the protection requirements of today's powerline equipment for general industrial use while also addressing the fast-growing need for solutions in the electrification of energy demand, catering to both consumer and commercial use.

As an increasing range of electrical and electronic equipment is required to meet electrical safety standards such as the IEC 62368-1, one notable advantage of the Model GDT28H Series is its suitability for use in AC isolation solutions. This is achieved through a combination of its extended operating voltage range, high insulation resistance, and heightened surge rate. These features give designers a space-saving solution that offers the same level of protection as a larger component. Additionally, the Model GDT28H Series offers a wider operating temperature range making it well-suited for applications in certain harsh conditions.

"Our Model GDT28H Series leverages Bourns' latest developments in GDT technology, enabling our customers to meet industry requirements for electrical safety across an ever-broadening variety of AC applications and appliances that can also benefit from its long service life," said David Chavarría, GDT/SPD Product Line Manager at Bourns. "We designed this next-generation series with features that deliver exceptional value to our customers, making it the preferred solution for general surge and isolation applications."

Bourns® Model GDT28H Series 2-electrode high voltage GDTs are available now and are RoHS compliant* and UL recognized. For more detailed product information, please see: www.bourns.com/products/circuit-protection/gas-discharge-tube-(gdt)-surge-arrestors/2-electrode-gdts/high-voltage-series/product/GDT28H

*RoHS Directive 2015/863, Mar 31, 2015 and Annex.

ボーンズ社について

ボーンズ社(Bourns, Inc.)は、パワーエレクトロニクス、抵抗素子、回路保護部品、およびセンシングソリューションを提供する株式非公開メーカーです。1947年に設立され、米国カリフォルニア州リバーサイドに本社を構え、グローバルな設計・製造・販売ネットワークを通じて、自動車、産業、民生、通信、医療†、オーディオ市場にサービスを提供しています。企業情報および製品情報の詳細は、www.bourns.comをご覧ください。

Bourns®およびBourns のロゴは、Bourns, Inc. の商標または登録商標であり、Bourns の許諾を得た場合のみ公的に使用することができ、また適切な権利の表記が必要です。 列挙した他の名称およびブランドは、各権利所有者の商標または登録商標です。

† Bourns®製品は、命を救うため、または生命を維持するためのアプリケーションや、Bourns®製品の故障または誤動作による人身傷害、または死亡につながる可能性のある、その他のアプリケーション向けに設計されていません。免責事項のお知らせをご参照ください。www.bourns.com/docs/legal/disclaimer.pdf